vl53l4cd variation in readings
- 1 reply
- 242 views
Hi,
We have incorporated a vl53l4cd into our product.
We wish to measure 0 to 100mm with a resolution of 1mm, and an update rate of at most 1 second.
We have set the vl53l4cd 19mm back from front measurement face (so we need to actually measure 19 to 119mm).
We placed statically on a desk I find, the variation of the readings to be from 33 to 40mm.
It does vary from reading to reading but the trend also varies so I cannot simply average it out.
Is this was what I should expect?
I attached a screenshot of what I find. This is against a light teak table. I would say is appears to better when against something black.
Is there any recommendations for settings for getting the best performance between 19 and 59mm in terms of stability (The inaccuracies are less significant beyond that)?
kind regards
Liam