Skip to main content
Visitor II
November 27, 2024
Question

VL53L4CD TOF sensor - need accuracy at 10 cm (or perhaps in range 5 - 20 cm)?

I am looking into the VL53L4CD TOF sensor but find the specifications on distance accuracy at 10 cm (or perhaps in range 5 - 20 cm) to be murky at best.  I need to be able to determine distance to object with accuracy of 0.02 mm (0.001 inches) at this distance and be able to determine if object has moved in or out by that amount or more.  

Can this device produce that kind of accuracy? Other posts here make me think not, that all it can do is about 1 mm.

Also, the ST introductory webinar mentioned higher resolution project 55H2 if I heard it right. 

Can you provide any insights on that? 

Or suggest another product that can provide the accuracy / precision that I need, please.

Initially planning to use Arduino for the CPU processing.

Thank you.

This topic has been closed for replies.

1 reply

Anne BIGOT
ST Technical Moderator
November 28, 2024

Hello

The accuracy of the VL53L4CD can be found in the table 17 of the datasheet. Unfortunately, the VL53L4CD accuracy is at least +/-6mm with a timing budget of 33ms on a 17% white target. 
With ToF it is today difficult to get an accuracy lower than 1mm.

If you want more details about the VD55H1, please contact the sales of your Region

Our community relies on fruitful exchanges and good quality content. You can thank and reward helpful and positive contributions by marking them as 'Accept as Solution'. When marking a solution, make sure it answers your original question or issue that you raised. ST Employees that act as moderators have the right to accept the solution, judging by their expertise. This helps other community members identify useful discussions and refrain from raising the same question. If you notice any false behavior or abuse of the action, do not hesitate to 'Report Inappropriate Content'