Skip to main content
Explorer II
April 1, 2024
Solved

VL53L4CD

Hi there,

I'm planning to integrate the VL53L4CD sensor into my custom board, which features the STM32G484CEU6 MCU.

After reviewing the datasheet, I found that the sensor operates within a voltage range of 2.6-3.5V (nom 2.8V). I just wanted to double-check if it's safe to connect this sensor directly to the MCU, considering that the I2C interface of the MCU is 3.3V.

Thank

This topic has been closed for replies.
Peter BENSCH
Peter BENSCHBest answer
ST Technical Moderator
April 1, 2024

Welcome @hbagheri, to the community!

Now, since 3.3V is in the range of 2.6V...3.5V, you can also supply the sensor from the 3.3V of the board and connect it directly via I2C.

Does it answer your question?

Regards
/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

2 replies

Peter BENSCH
Peter BENSCHBest answer
ST Technical Moderator
April 1, 2024

Welcome @hbagheri, to the community!

Now, since 3.3V is in the range of 2.6V...3.5V, you can also supply the sensor from the 3.3V of the board and connect it directly via I2C.

Does it answer your question?

Regards
/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
John E KVAM
ST Employee
April 1, 2024

I have a quicker answer - YES. 3v3 is just fine. Do try not to over-voltage it though. Cuts down on the lifetime. 

But 3v3 is well tested and will work for you.

- john

If this or any post solves your issue, please mark them as 'Accept as Solution' It really helps. And if you notice anything wrong do not hesitate to 'Report Inappropriate Content'. Someone will review it.