Associate II
April 8, 2023
Question
VL53L3CX: estimating target distance from histogram
- 3 replies
- 2206 views
I have attached a couple of histograms from same object and from different distances. Distances are embedded in filename visible in image (top bar). Problem is peak position doesn’t change. I understand depth data is spread across three bins only. But how possibly does the peaks only happen at one position.
NB: the extra peaks on the far right for some of the histograms I presume to be as result of reflection.
can anyone help clarify how to see objects distances let’s say in meters (as max distance is 4m) ?
also if this is not possible I’d like some clarification about why.
v++