The sensors do not interfere with each other when pointed at different angles.
So if one sensor covered one 45 degree area and the other covered a different 40 degree area, it would work just fine. For sure some of the light from sensor A would get into sensor B, but that light would be treated as ambient discounted.
A VL53L5 covers a 45x45 versus the 20x20 that the VL53L1 covers.
The L5 is more expensive, but it's not 2X the L1, so switching to the VL53L5 in this case makes a lot of sense.
You also get simultaneous zone information, which could be a plus.
If this or any post solves your issue, please mark them as 'Accept as Solution' It really helps. And if you notice anything wrong do not hesitate to 'Report Inappropriate Content'. Someone will review it.