Skip to main content
Visitor II
June 12, 2024
Question

VL53L1X status 9

I can't find any information about status 9, how can I resolve this status?

This topic has been closed for replies.

1 reply

John E KVAM
ST Employee
June 17, 2024

That's because we hide the user manual. 

When you download the driver from ST.com It's:

 

STSW-IMG009

VL53L1X ULD API (Ultra Lite Driver application programming interface)

Start with this one - it's probably closer to what you have.

There is also a full version. It is:

STSW-IMG007

VL53L1X full API (application programming interface and documentation)

The user manual is in with the code.

Anyway, a range status of 9 is 'signal failure'. Not enough photons were returned to get a valid range. 

you can adjust this as you get to pick the minimum number of photons you determine is 'enough'.

Even if you don't use the ST driver. Download the code to get the user manual.

- john

If this or any post solves your issue, please mark them as 'Accept as Solution' It really helps. And if you notice anything wrong do not hesitate to 'Report Inappropriate Content'. Someone will review it.