Skip to main content
Associate
August 15, 2023
Solved

VL53L1X SATEL - does the PCB plug of the Mini-PCB match any standard?

If I want to use the Mini-PCB of the VL53L1X SATEL, which type of plug do I need to plug that in?

(I would like to label this with "Time of flight" but unfortunately, this seems to be not possible for me ;-( ).

This topic has been closed for replies.
Zhiyuan.Han
Zhiyuan.HanBest answer
ST Technical Moderator
August 29, 2023

Hi AchimKraus

For VL53L1-SATEL, actually there are two connector you can use, either the 2.54mm dual-line pin header, this is standard connector; or you can use the golden finger pin at the other side.

The golden pin is mainly used for flying wire and not designed for a specific connector, the target of this break board is to make it as small as possible, with small size, it will be easier to put it inside customer housing for function evaluation. 

 

 

Br

Zhiyuan.Han

 

 

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.

7 replies

Zhiyuan.Han
ST Technical Moderator
August 16, 2023

Hi 

VL53L1X SATEL is designed for easy integration into customer devices, the plug connector is designed for VL53L1X expansion board. for more detail information, please check below link on the VL53L1X-SATEL user manual. 

Data brief - VL53L1X-SATEL - Breakout boards based on the VL53L1X long distance ranging Time-of-Flight sensor

 

br

Zhiyuan.Han

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
Associate
August 18, 2023

> VL53L1X SATEL is designed for easy integration into customer devices

Maybe, but that document doesn't contain information about that plug (the one the PCB builds on its own). Without that information, "easy" is something else.

 

Anne BIGOT
ST Technical Moderator
January 11, 2024

Indeed on st.com, the BOM of the board is missing.

Here is the link to the reefrence of the header used on the SATEL.

SSQ-103-01-T-D - Tiger Buy™ Socket Strip with Square Tails, 0.100" Pitch | Samtec

Our community relies on fruitful exchanges and good quality content. You can thank and reward helpful and positive contributions by marking them as 'Accept as Solution'. When marking a solution, make sure it answers your original question or issue that you raised. ST Employees that act as moderators have the right to accept the solution, judging by their expertise. This helps other community members identify useful discussions and refrain from raising the same question. If you notice any false behavior or abuse of the action, do not hesitate to 'Report Inappropriate Content'
Associate
January 11, 2024

My question focus on the "golden finger pin" , the other one, the 2.54mm dual-line pin header, is easy to find.