Skip to main content
KArai.2
Associate II
November 17, 2022
Solved

VL53L1X Boot period specs (setup time from hardware standby to SW standby)

Hello,

​

I am developing a system using VL53L1X.

Occasionally, when the host microcomputer is asynchronously reset, 

there is no response from the sensor after that.

​

I've never used the xshut terminal.

If communication with the sensor becomes impossible, 

I'm thinking of using the xshut terminal to synchronize the host microcomputer and the sensor.

Please let me know the setup time required to start I2C communication after setting the xshut pin to high level.

​

From the topic below, I think 10ms is enough, but I would like some information as a specification.

Title:vl53l1x-xshut-pin

​

​

Best regards.

This topic has been closed for replies.
John E KVAM
John E KVAMBest answer
ST Employee
November 17, 2022

It's a lot less than 10ms. But you don't need to know it.

drop Xshut, wait a ms or two and lift the Xshut line.

The sensor will reboot and come alive.

There is a I2C read -

VL53L1X_ERROR VL53L1X_BootState(VL53L1_Dev_t dev, uint8_t *state)

Just call that.

If it's not booted, wait a ms and call it again.

If this or any post solves your issue, please mark them as 'Accept as Solution' It really helps. And if you notice anything wrong do not hesitate to 'Report Inappropriate Content'. Someone will review it.

2 replies

John E KVAM
John E KVAMBest answer
ST Employee
November 17, 2022

It's a lot less than 10ms. But you don't need to know it.

drop Xshut, wait a ms or two and lift the Xshut line.

The sensor will reboot and come alive.

There is a I2C read -

VL53L1X_ERROR VL53L1X_BootState(VL53L1_Dev_t dev, uint8_t *state)

Just call that.

If it's not booted, wait a ms and call it again.

If this or any post solves your issue, please mark them as 'Accept as Solution' It really helps. And if you notice anything wrong do not hesitate to 'Report Inappropriate Content'. Someone will review it.
KArai.2
KArai.2Author
Associate II
November 18, 2022

Hello John-san,

Thank you for your answer.

I will try it on a real device to determine the setup time.

The information "about 1ms-2ms range" was very helpful.

Best regards.