Skip to main content
JPere.3
Associate II
May 16, 2020
Solved

VL53L1X - Autonomous low-power mode

If anyone could help me point to location in the API where I could implment "Autonomous low-power mode".

And on "Autonomous low-power mode" what is the expected current draw?

for a battery operated project what should I tweak in the API to get more power savings?

Thanks in advance.

This topic has been closed for replies.
John E KVAM
John E KVAMBest answer
ST Employee
May 18, 2020

Autonomous means that the sensor will work while your MCU is asleep waiting for an interrupt.

You can configure thresholds that will tell the sensor under what conditions the sensor will trigger the interrupt.

If running continuously the sensor will draw 20mA.

By setting the timing budget and intermeasurement period, you can greatly reduce the power consumption.

By ranging once per second (use intermeasurement period of 1 second) and ranging for only 15ms (Timing budget = 15ms) you will use:

20mA *15ms *1 range = 20 x 0.015 = 0.3mA.

By default the sensor will range until you tell it to stop.

so your MCU can go to sleep secure in the knowledge you will get the interrupt if something comes close (if that's how you set up the interrupt.)

One clever trick. You can use a laptop camera or a non-iPhone camera to see the sensor still at work. The rather poor IR filter on the camera will turn the invisible flash into a visible flash.

If this or any post solves your issue, please mark them as 'Accept as Solution' It really helps. And if you notice anything wrong do not hesitate to 'Report Inappropriate Content'. Someone will review it.

2 replies

John E KVAM
John E KVAMBest answer
ST Employee
May 18, 2020

Autonomous means that the sensor will work while your MCU is asleep waiting for an interrupt.

You can configure thresholds that will tell the sensor under what conditions the sensor will trigger the interrupt.

If running continuously the sensor will draw 20mA.

By setting the timing budget and intermeasurement period, you can greatly reduce the power consumption.

By ranging once per second (use intermeasurement period of 1 second) and ranging for only 15ms (Timing budget = 15ms) you will use:

20mA *15ms *1 range = 20 x 0.015 = 0.3mA.

By default the sensor will range until you tell it to stop.

so your MCU can go to sleep secure in the knowledge you will get the interrupt if something comes close (if that's how you set up the interrupt.)

One clever trick. You can use a laptop camera or a non-iPhone camera to see the sensor still at work. The rather poor IR filter on the camera will turn the invisible flash into a visible flash.

If this or any post solves your issue, please mark them as 'Accept as Solution' It really helps. And if you notice anything wrong do not hesitate to 'Report Inappropriate Content'. Someone will review it.
JPere.3
JPere.3Author
Associate II
May 18, 2020

Thanks John.