Skip to main content
Associate
Jul 28, 2025 6:50 AM UTC
Question

VL53L1X Accuracy Issue with Dark Clothing , Should I Switch to VL53L5CX?

Hi,

I'm working on a people counting system using the VL53L1X in multi-zone mode with a single sensor. It works well in general, but I'm seeing accuracy issues when people wear black or dark clothing—likely due to low reflectivity.

I’d appreciate some guidance:

  • Would the VL53L5CX provide better detection for dark clothing?

  • Does it handle low-reflectivity surfaces more reliably?

  • Or would it be better to use multiple VL53L1X sensors?

  • Any other sensor recommendations for more reliable people detection?

Thanks in advance!
Basil

This topic has been closed for replies.

2 replies

Graduate
Jul 31, 2025 3:23 AM UTC

Basil - 

the VL53L5 is one choice, but a better idea would be to go with the VL53L8CX. 

The L8CX has better optics that allows a more powerful VCSEL (Laser) output. 

And because ST actually makes the optics out of Silicon Wafers, the cost for the L8 is the same as for the L5. 

So you get a better sensor - which will detect people to a greater distance - for the same price as for the VL53L5.

It is unfortunately more costly than the L1CX, but worth every penny. I'm sure it will do what you need.

- John (ST Retired.)

"If this or any post solves your issue, please mark them as ""Accept as Solution"". It really helps the next guy.And if you notice anything wrong do not hesitate to ""Report Inappropriate Content"".I am a recently retired ST Employee. My former username was John E KVAM."
BasilAuthor
Associate
Aug 1, 2025 4:38 AM UTC

Hi John,

Thank you so much for the helpful recommendation!

Just a quick follow-up: For a bidirectional people counter, would the VL53L8CX alone be sufficient to reliably detect direction as well, or would I still need to combine it with another sensor (e.g., another ToF or ultrasonic) to improve accuracy?

Also, are there any limitations or considerations I should be aware of when using the VL53L8CX for bidirectional counting—especially in high-traffic or low-reflectivity scenarios?

Additionally, would you recommend any specific mounting orientation or zone configuration that tends to work best for tracking directional movement?

Appreciate your insights!

Best,
Basil