Skip to main content
Associate II
February 8, 2025
Question

VL53L1_ERROR_ZONE_GPH_ID_CHECK_FAIL

We found a problem with VL53L1CB, After VL53L1_GetMeasurementDataReady returns 0, VL53L1_GetMultiRangingData returns VL53L1_ERROR_ZONE_GPH_ID_CHECK_FAIL. What causes this problem?

Thank anyone for a little help

This topic has been closed for replies.

3 replies

John E KVAM
ST Employee
February 10, 2025

I think you want VL53L1_GetMeasurementDataReady to return a 1 to indicated that a measurement was ready. 

I believe that error will go away once the measurement is actually ready. Although I did not find any useful references to it in the code. (There is just the function that translates the error to a string - which is not really helpful.)

Try starting the sensor and waiting a good long (At least whatever you have set for Timing Budget) time before calling VL53L1_GetMeasurementDataReady. You will know the sensor has finished, and you will know what VL53L1_GetMeasurementDataReady is supposed to return when done.

- john

If this or any post solves your issue, please mark them as 'Accept as Solution' It really helps. And if you notice anything wrong do not hesitate to 'Report Inappropriate Content'. Someone will review it.
User.120Author
Associate II
February 11, 2025

Thank you very much for your response.

VL53L1_GetMultiRangingData(VL53L1_DEV Dev, VL53L1_MultiRangingData_t *pMultiRangingData) *pMultiRangingData in this function returns 1, I also waited until *pMultiRangingData was 1 before executing VL53L1_GetMultiRangingData. So I don't know why this result is returned.

In addition, I want to determine whether the ranging performance under the drive of STSW-IMG019 is LONG>MEDIUM>SHORT. I see MEDIUM>LONG>SHORT in um2133, and the actual test is LONG>MEDIUM>SHORT.

Thank anyone for a little help

 

Zhiyuan.Han
ST Technical Moderator
June 19, 2025

Hi 

About the code sequence, I attach the example code here, you need to check NewDataReady with VL53L1_GetMeasurementDataReady(), if the NewDataReady return 1, that means ranging data ready, and you can read the ranging data VL53L1_GetMultiRangingData().

 do{ // polling mode
 status = VL53L1_GetMeasurementDataReady(Dev, &NewDataReady);
 HAL_Delay(1);
 if((!status)&&(NewDataReady!=0)){
 status = VL53L1_GetMultiRangingData(Dev, pMultiRangingData);
 no_of_object_found=pMultiRangingData->NumberOfObjectsFound;
 printf("Count=%5d, ", pMultiRangingData->StreamCount);
 printf("#Objs=%1d ", no_of_object_found);
 for(j=0;j<no_of_object_found;j++){
 if(j!=0)printf("\n ");
 printf("status=%d, D=%5dmm, Signal=%2.2f Mcps, Ambient=%2.2f Mcps",
 pMultiRangingData->RangeData[j].RangeStatus,
 pMultiRangingData->RangeData[j].RangeMilliMeter,
 pMultiRangingData->RangeData[j].SignalRateRtnMegaCps/65536.0,
 pMultiRangingData->RangeData[j].AmbientRateRtnMegaCps/65536.0);
 }
 printf ("\n");
 if (status==0){
 status = VL53L1_ClearInterruptAndStartMeasurement(Dev);
 }
 }
 }
 while (1);

 

Br

Zhiyuan.Han

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.