Skip to main content
Gaston
Associate III
October 25, 2023
Question

VL53L0CXV0DH/1 issue after production

I've manufactured 160 boards implementing the VL53L0CXV0DH/1. Many work as expected but some of them (approximately 50 units) give 8191 always as a result. I've noticed that these devices should be treated carefully using a recommended reflow profile. Also they are susceptible to shock damage.

What could be the cause of the result being 8191, in those defective devices?

Gaston_0-1698267119207.png

thanks in advance,
gaston

This topic has been closed for replies.

1 reply

Zhiyuan.Han
ST Technical Moderator
January 11, 2024

Hi Gaston

Normally 8191 means no target was detected, is it possible to log more information from RangingMeasurementData to help understand your issue? such as return signal rate, range status etc. 

 

ZhiyuanHan_0-1704939706117.png

 

Br

Zhiyuan.Han

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.