Skip to main content
Visitor
Jul 25, 2026 4:08 PM UTC
Solved

VD5943 – MIPI CSI-2 Clock Mode (Continuous vs Non-Continuous)

Hello,

I am integrating the VD5943 image sensor with a Lattice FPGA acting as a MIPI CSI-2 receiver.

I have reviewed both the VD5943 Datasheet (DS14968) and the Reference Manual (RM0532), but I could not find any information about the operating mode of the MIPI CSI-2 clock lane.

Could someone from ST please clarify the following?

  • Does the VD5943 transmit the MIPI CSI-2 clock in Continuous Clock mode or Non-Continuous Clock mode?
  • If this behavior is configurable, which register controls it?
  • If it is fixed, which mode is implemented by default?

This information is important to ensure compatibility with our FPGA CSI-2 receiver and downstream processing.

Thank you for your support.

AdrienBonnatBest answer
ST Technical Moderator
Jul 29, 2026 12:12 PM UTC

Hello,

The VD5943 is using continuous clock by default. The mode can be selected through bit 4 of debug register DPHYTX_CTRL at address 0x108c, please refer to table 14 of register manual.

Best regards

Adrien

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.

1 reply

AdrienBonnatBest answer
ST Technical Moderator
Jul 29, 2026 12:12 PM UTC

Hello,

The VD5943 is using continuous clock by default. The mode can be selected through bit 4 of debug register DPHYTX_CTRL at address 0x108c, please refer to table 14 of register manual.

Best regards

Adrien

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.