Skip to main content
3FTI
Associate III
Jun 10, 2025 1:55 PM UTC
Solved

VD563 error building libcamera from en.STSW-IMG502_RPI.zip source

I am trying to build the libcamera from the source files provided in "en.STSW-IMG502_RPI.zip" and I am getting the following error. I have cloned https://github.com/raspberrypi/libcamera.git and confirmed I can successfully build it to verify I have installed all the necessary tools.

Here is the output from the meson setup command:

$ sudo meson setup build --buildtype=release -Dpipelines=rpi/vc4,rpi/pisp -Dipas=rpi/vc4,rpi/
pisp -Dv4l2=enabled -Dgstreamer=disabled -Dtest=false -Dlc-compliance=disabled -Dcam=disabled -Dqcam=disabled -Ddocumentation=disabled -Dpycamera=enabled
The Meson build system
Version: 1.5.1
Source dir: /home/chad/stcam/STSW-IMG502_RPI/STSW-IMG502_RPI_v.0.5.0/libcamera0.5_0.5.0+rpt20250429+st20250606/src
Build dir: /home/chad/stcam/STSW-IMG502_RPI/STSW-IMG502_RPI_v.0.5.0/libcamera0.5_0.5.0+rpt20250429+st20250606/src/build
Build type: native build
Project name: libcamera
Project version: 0.5.0
C compiler for the host machine: cc (gcc 12.2.0 "cc (Debian 12.2.0-14+deb12u1) 12.2.0")
C linker for the host machine: cc ld.bfd 2.40
C++ compiler for the host machine: c++ (gcc 12.2.0 "c++ (Debian 12.2.0-14+deb12u1) 12.2.0")
C++ linker for the host machine: c++ ld.bfd 2.40
Host machine cpu family: aarch64
Host machine cpu: aarch64
Header "fcntl.h" has symbol "F_ADD_SEALS" : YES
Header "unistd.h" has symbol "issetugid" : NO
Header "locale.h" has symbol "locale_t" : YES
Header "sys/mman.h" has symbol "memfd_create" : YES
Header "stdlib.h" has symbol "secure_getenv" : YES
Compiler for C supports arguments -Wno-c99-designator: NO
Found pkg-config: YES (/usr/bin/pkg-config) 1.8.1
Found CMake: /usr/bin/cmake (3.25.1)
Run-time dependency lttng-ust found: NO (tried pkgconfig and cmake)
Program ./parser.py found: YES (/usr/bin/python3 /home/chad/stcam/STSW-IMG502_RPI/STSW-IMG502_RPI_v.0.5.0/libcamera0.5_0.5.0+rpt20250429+st20250606/src/utils/codegen/ipc/./parser.py)
Program ./generate.py found: YES (/usr/bin/python3 /home/chad/stcam/STSW-IMG502_RPI/STSW-IMG502_RPI_v.0.5.0/libcamera0.5_0.5.0+rpt20250429+st20250606/src/utils/codegen/ipc/./generate.py)
Program ./extract-docs.py found: YES (/usr/bin/python3 /home/chad/stcam/STSW-IMG502_RPI/STSW-IMG502_RPI_v.0.5.0/libcamera0.5_0.5.0+rpt20250429+st20250606/src/utils/codegen/ipc/./extract-docs.py)

utils/meson.build:4:0: ERROR: Nonexistent build file 'utils/ipu3/meson.build'

 

This topic has been closed for replies.
MeganeG
MeganeGBest answer
ST Technical Moderator
Jun 26, 2025 9:32 PM UTC

Hello @3FTI,

Indeed, it appears that some files were lost during the repackaging of the archive. We apologize for this issue. The problem has now been resolved and the updated version is available on our website. If you download the latest version now, you should have all the files. Please let us know if you encounter any further issues.

Thanks, Megane

 

 

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.

2 replies

MeganeG
MeganeGBest answer
ST Technical Moderator
Jun 26, 2025 9:32 PM UTC

Hello @3FTI,

Indeed, it appears that some files were lost during the repackaging of the archive. We apologize for this issue. The problem has now been resolved and the updated version is available on our website. If you download the latest version now, you should have all the files. Please let us know if you encounter any further issues.

Thanks, Megane

 

 

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.
3FTI
3FTIAuthor
Associate III
Jul 2, 2025 7:52 PM UTC

Thanks that did it!