Skip to main content
RFitc
Visitor II
April 11, 2019
Question

URGENT! How to I change the roi (fov) to 15 deg. or 4x4 array on the VL53L1X Tof Sensor on Raspberry Pi 3B?

Everywhere I look, the VL53L1X Tof Sensor says that it has a standard fov of 27 degrees (or 16x16) and can be reduced to 15 degrees (or 4x4 SPAD array). But how do I do this on the Raspberry Pi (in python)? In your VL53L1X_register_map.h there is a function called:

#define VL53L1_ROI_CONFIG__MODE_ROI_XY_SIZE 0x013F
 
/*!<
 
 type: uint8_t \n
 
 default: 0x00 \n
 
 info: \n
 
 - msb = 7
 
 - lsb = 0
 
 - i2c_size = 1
 
 groups: \n
 
 ['nvm_copy_data', 'roi_config']
 
 fields: \n
 
 - [7:0] = mode_roi_xy_size
 
*/

How do I use this or another function to make my ROI 15 degrees (4x4 SPAD) instead of 27 on the Raspberry Pi like your documentation says it can? Or do I have to hook it up to some software and do it in there to change it?

This topic has been closed for replies.

1 reply

John E KVAM
ST Employee
April 16, 2019

Quickly download the UltraLitte driver from ST.com - STSW-IMG009.

The code in here is very simple. You can use that as an example.

If this or any post solves your issue, please mark them as 'Accept as Solution' It really helps. And if you notice anything wrong do not hesitate to 'Report Inappropriate Content'. Someone will review it.