Associate
October 31, 2023
Solved
Unable to connect with vl53L7CX SATEL using STM32 L432 KC
- 7 replies
- 3754 views
Hi guys!
From the last week I am trying to connect my TOF sensor with the STM32, but the I2C Communication has not been started. I have tried to use I2C Scanner to scan the address of the VL53L7CX SATEL breakout board but was not even able to gets its address back. I also tried changing the VL53L7CX SATEL breakout board but it was also not very useful. I have tried using both the STM32 Cube Ide software package that they provide for the TOF Sensosrs and the STM32duino VL53L7CX Library but was unsuccessful in making them work.
Can anyone let me know if I am making any mistakes or if my approach is wrong in any way!
Thank you in advance!