Skip to main content
umer.q
Associate
June 18, 2022
Question

ToF VL53L3CX IO (IOVDD) Standard mode VS 2V8 mode voltage levels.

Hi,

I am using VL53L3X with MPU having voltage level 1.8V. In the data sheet it is mentioned that IOVDD typical voltage level is 1.8V in standard mode and 2.8V in 2.8V mode.

I want to make sure my design is correct to use VL53L3CX in 1.8V standard mode.

0693W00000NsEMBQA3.png 

This topic has been closed for replies.

4 replies

John E KVAM
ST Employee
June 21, 2022

Redacted. I was looking at a datasheet for the wrong chip.

-john

If this or any post solves your issue, please mark them as 'Accept as Solution' It really helps. And if you notice anything wrong do not hesitate to 'Report Inappropriate Content'. Someone will review it.
umer.q
umer.qAuthor
Associate
June 21, 2022

Hi John,

Thank you for the help.

I did not find any VDDIO PIN for VL53L3X in datasheet.

Can you tell me specific PIN for VDDIO in below image.

Thank you.

0693W00000NsOLXQA3.png

umer.q
umer.qAuthor
Associate
June 21, 2022

0693W00000NsOLwQAN.pngAbove is the Application schematic from Datasheet.

I have connected IOVDD to 1.8V and AVDD to 2.8V.

John E KVAM
ST Employee
June 21, 2022

for an input on GPIO1, min is 0.7 times IOVDD. So that's fine. Input high has to be 1.12v min on I2C. So that is is fine as well. You are not the first. And the others worked well.

So go ahead.

  • john
If this or any post solves your issue, please mark them as 'Accept as Solution' It really helps. And if you notice anything wrong do not hesitate to 'Report Inappropriate Content'. Someone will review it.