Skip to main content
MBaum.7
Associate III
November 29, 2023
Solved

TOF sensor: Distinguish between multiple reflective surfaces

  • November 29, 2023
  • 1 reply
  • 2299 views

Used sensor: VL53L1X

Application: TOF sensor is on bottom of a liquid filled container to measure the fill level. The light of the TOF-sensor is reflected on:

1) Liquid surface (water to air, oil to air)

2) Container roof surface

Is it possible to mask out one of the reflective surfaces by limit the accepted distance for the measurement (or better: time of flight) to an expected range?

E.g: The red light in the sketch will have a longer 'travel time' as the magenta light because the time to travel trough the air volume is added. If I could mask the sensor to 'see' only times below/above a given limit, I could mask out one of the reflective surfaces.

MBaum7_0-1701242349554.png

 

This topic has been closed for replies.
Best answer by Anne BIGOT

Hello,

Using VL53L1X it is not possible to distinguish between the two surfaces.
One option could  be to use histograms sensors like VL53L1CB or VL53L7CH or VL53L8CH.
It the condition of a VL53L1CB, the minimum distance between the two surfaces should be 80cm.

In the case of the VL53L7CH or VL53L8CH, the minimum distance between the two surfaces should be 60cm.

Regards

1 reply

Anne BIGOT
Anne BIGOTBest answer
Technical Moderator
December 4, 2023

Hello,

Using VL53L1X it is not possible to distinguish between the two surfaces.
One option could  be to use histograms sensors like VL53L1CB or VL53L7CH or VL53L8CH.
It the condition of a VL53L1CB, the minimum distance between the two surfaces should be 80cm.

In the case of the VL53L7CH or VL53L8CH, the minimum distance between the two surfaces should be 60cm.

Regards

Our community relies on fruitful exchanges and good quality content. You can thank and reward helpful and positive contributions by marking them as 'Accept as Solution'. When marking a solution, make sure it answers your original question or issue that you raised. ST Employees that act as moderators have the right to accept the solution, judging by their expertise. This helps other community members identify useful discussions and refrain from raising the same question. If you notice any false behavior or abuse of the action, do not hesitate to 'Report Inappropriate Content'