Skip to main content
Associate II
June 19, 2024
Question

ToF inaccuracy

Hi,

 

I was doing a distance test on the VL53L4CX sensor using ESP32 and the ST example codes on Arduino. I'm getting  inconsistent offset errors across the range. The setup is a brine tank with salt inside it. Any ideas on this?

 

Thank you.

This topic has been closed for replies.

6 replies

John E KVAM
ST Employee
June 20, 2024

When looking at water (briny or not) you have a problem with light penetrating the liquid, being slowed down, hitting the bottom of the tank and reflecting. If the liquid is deeper than about 15 cm, or if you paint the bottom with a non-reflective coating, this effect goes away.

Could you run the experiment again putting more than 15cm of water in the bucket?

Looking at your data, I'm going to guess you added some liquid to a bucket, then lifted your sensor and took measurement. So, the bottom might have an 'offset' effect. Both sensors over-range by about the same amount (except at 600 - that data point is an outlier. 

I going to guess that maybe you did NOT do an offset calibration before you started. That might account for all your numbers being low.

JohnEKVAM_0-1718900391639.png

Try doing an offest cal on your sensors - see what it tells you. If you get 20mm of offset, I'd say the numbers looks as good as they can. (Just update your data by the offset amount and have another look.)

I'm not sure I can explain the data point at 600 though. Experimental error. 

Try it again with a deeper pool of water, and doing the calibration. Then we can re-visit the numbers.

- john 

 

 

If this or any post solves your issue, please mark them as 'Accept as Solution' It really helps. And if you notice anything wrong do not hesitate to 'Report Inappropriate Content'. Someone will review it.
karlachaAuthor
Associate II
June 25, 2024

Thank you, John. Our measurements are taken only during after fill so it's totally dry. I took another test using two similar hardware and here are the results.

karlacha_0-1719327269539.png

 

John E KVAM
ST Employee
June 25, 2024

there are lots of reasons to under-range. Coverglass being the main culprit. But OVER-ranging - especially by this much is a completely new one on me. Is it possible that you are using crosstalk correction but have removed the coverglass? It's really all I can think of. Or somehow you did the offset correction and got the sign wrong direction?

To be off by 100+ is basically impossible. 

Could it be that your target is small and the 18-degree FoV is seeing something in the background that is getting averaged in? (The diameter of the target should be at least 1/3 of your max distance. So at 600mm, the diameter should be at least 20cm. 

Can you add a picture of your setup? Something is really odd.

- john

If this or any post solves your issue, please mark them as 'Accept as Solution' It really helps. And if you notice anything wrong do not hesitate to 'Report Inappropriate Content'. Someone will review it.
karlachaAuthor
Associate II
June 27, 2024

Hi John,

 

It's a 600-m deep tank. It has a little salt in it with no water. I'm suspending the unit with a fishing line so I could reel in every 10 cm. The Pentair unit is just for reference.

 

Thanks