Skip to main content
RChen.1654
Associate II
December 19, 2019
Question

There is no RefSPAD calibration in VL53L1X ULD driver. How to peform RefSPAD calibration if VL53L1X ULD driver is used ?

..

This topic has been closed for replies.

2 replies

John E KVAM
ST Employee
December 19, 2019

​Experimental results showed that the RefSPAD did not improve the range as much as we thought it was.

In the end, the sensor works fine without it.

If this or any post solves your issue, please mark them as 'Accept as Solution' It really helps. And if you notice anything wrong do not hesitate to 'Report Inappropriate Content'. Someone will review it.
RChen.1654
Associate II
December 20, 2019

From document, it says that RefSPAD and crosstalk calibrations have to be performed whenever the customer adds a protective cover glass on top of the VL53L1X module. So the VL53L1X ULD driver can solve the case that a protective cover glass is on top of the VL53L1X module, right?

Is there other performance risks if we select the VL53L1X ULD driver because it is easy to port on Android platform?