Skip to main content
Associate II
January 3, 2024
Question

The relationship between the sequence number of Zone mapping in VL53L5C and the returned result

There is an explanation about Zone mapping in the document as follows :

123.png

 The area number in the above figure is consistent with the example VL53L5CX_ How do the return results in VL53L5CX_SimpleRanging ?

In VL53L5CX_SimpleRanging ,There is the following code:

(long)Result->ZoneResult[j + k].Distance[l],

I printed the output of [j + k](Taking 4 * 4 as an example):3 2 1 0  7 6 5 4 11 10 9 8 15 14 13 12 

Is this value of [j + k] the corresponding area number?

This topic has been closed for replies.

1 reply

John E KVAM
ST Employee
January 7, 2024

Use the GUI on the Evaluation kit. You can see the zone numbering. But yes, the 0,0 bin is in the upper right, assuming your perspective is looking at the chip from the ranging side, and NOT as if you were standing in back of the sensor.

 

If this or any post solves your issue, please mark them as 'Accept as Solution' It really helps. And if you notice anything wrong do not hesitate to 'Report Inappropriate Content'. Someone will review it.