Question
STEVAL-66GYMAI1 Incorrect Lens
- 1 reply
- 12 views
Similar to this post earlier this year, the same setup using the STM32N657x0-Q + STEVAL-66GYMAI1 seems to have the wrong lens shipped on the order. When streaming video, the only distance with a in-focus image is from extremely close up (<2 cm), which is not what is advertised for the STEVAL-66GYMAI1. The attached photo shows an example of the camera pointed at the dev board showing this issue. When adjusting the M12 lens focus across its full rotation range, no improvements were made.