Visitor II
September 27, 2022
Question
ST VL53L3CX TOF Sensor - Wrong Measurement in Water Level Sensing.
- 1 reply
- 1919 views
Dear ST and Team,
Am using ST's VL53L3CX STEL Board for water level sensing project prototyping. I Have Queries following below
- is VL53L3CX is suitable for water level sensing ?
- do we need any calibration for accuracy ?
- i have generated code simple raging application using STCubeMx (Using STM32F103RCT6 Controller ). is simple ranging application can also measure water level ?
- While detecting object am getting almost better accuracy distance, while distance is increasing of object from accuracy is becoming low. +- 20mm is for upto 1000 mm target is getting. how to increase the accuracy ?
- While testing for Water detection, Some times distance is showing totally wrong and some times distance accuracy is +- 10mm for 150mm target.
- i have tested in multiple containers like Glass, Jug and Bucket. but not able to read correct values.
- am using some cables for interfacing the VL53L3Cx. attaching the pic. Does it anything wrong using some length cable ?
I am sharing some pics for your reference. Please Help me out.