Skip to main content
Associate
April 2, 2025
Solved

Setting up X-NUCLEO-53L5A1

Hi, I have X_NUCLEO-53L5A1 expansion board. I connected this board to ESP8266 inorder to use the VL53L5CX sensor. But the sensor is not being detected.

#include <Wire.h>

void setup() {
 Serial.begin(115200);
 Wire.begin(4, 5); // GPIO4 (SDA), GPIO5 (SCL)

 Serial.println("\nI2C Scanner - Searching for devices...");
}

void loop() {
 byte error, address;
 int nDevices = 0;

 Serial.println("Scanning...");

 for (address = 1; address < 127; address++) {
 Wire.beginTransmission(address);
 error = Wire.endTransmission();

 if (error == 0) {
 Serial.print("I2C device found at address 0x");
 Serial.println(address, HEX);
 nDevices++;
 }
 }

 if (nDevices == 0) Serial.println("No I2C devices found.");
 else Serial.println("Scan complete.");

 delay(5000); // Repeat scan every 5 seconds
}

 

I get an output saying no devices found. After researching about it, I found that the sensor is not enabled. How do I enable the sensor and make it work. 

 

Connections:

X_NUCLEO-53L5A1            ESP8266

SCL                                       GPIO 5

SDA                                      GPIO 4

3V3                                       3V3

GND                                     GND

 

Please help me I am totally new to this. Thanks in advance.

This topic has been closed for replies.
John E KVAM
John E KVAMBest answer
ST Employee
April 2, 2025

There are lots of things that can go wrong - but it's after you start talking to the chip. If you cannot even find it, you have one of two issues. 1) no power or 2) your LPn line is low. I suppose you might have the clock and data pins backward - but that's pretty much it. 

There are 2 processors in the sensor. One does the ranging, the other does the I2C interface. 

It's really hard to stop the I2C from working. That bit of IP has been around for a really long time. It works.

So double check. You have a hardware error.

- john

 

 

If this or any post solves your issue, please mark them as 'Accept as Solution' It really helps. And if you notice anything wrong do not hesitate to 'Report Inappropriate Content'. Someone will review it.

4 replies

John E KVAM
John E KVAMBest answer
ST Employee
April 2, 2025

There are lots of things that can go wrong - but it's after you start talking to the chip. If you cannot even find it, you have one of two issues. 1) no power or 2) your LPn line is low. I suppose you might have the clock and data pins backward - but that's pretty much it. 

There are 2 processors in the sensor. One does the ranging, the other does the I2C interface. 

It's really hard to stop the I2C from working. That bit of IP has been around for a really long time. It works.

So double check. You have a hardware error.

- john

 

 

If this or any post solves your issue, please mark them as 'Accept as Solution' It really helps. And if you notice anything wrong do not hesitate to 'Report Inappropriate Content'. Someone will review it.
Associate
April 2, 2025

Thank you John, I will surely check on it. 

Associate
April 2, 2025

Do I need to configure anything using the NUCLEO-F4014E and software, because I saw many posts using the NUCLEO-F4014E board.