Skip to main content
Associate II
Aug 25, 2025 2:27 PM UTC
Question

Running two Adafruit VL53L4CD with Arduino R4 WiFi

I've been trying to get two Adafruit VL53L4CD's to work without a multiplexer on my Arduino R4 WiFi, and am getting stuck after getting one reading. I'm largely drawing on the code discussed here, and have also changed up the bits that nh1628 discussed at the end of the thread so that it matched. I am not sure why it seemed to work for them, but not in my case:

 

#include <Arduino.h>
#include <Wire.h>
#include <vl53l4cd_class.h>
#include <string.h>
#include <stdlib.h>
#include <stdio.h>
#include <stdint.h>
#include <assert.h>
#include <stdlib.h>

// Define I2C bus
#define DEV_I2C Wire
// Define Serial Port
#define SerialPort Serial

// Define Built-IN LED
#ifndef LED_BUILTIN
 #define LED_BUILTIN 13
#endif
#define ledPin LED_BUILTIN

// set the pins to shut down the sensors so we can assign addresses one by one
#define gpio_pin_1 4
#define xshut_pin_1 5
#define gpio_pin_2 6
#define xshut_pin_2 7
#define GFX_BL DF_GFX_BL

// Addresses for Sensors
uint8_t sensor_1_address = 0x51;
uint8_t sensor_2_address = 0x28;

volatile int interruptCount = 0;

void measure() {
 interruptCount = 1;
}

// Report Storage Structure
char report[64];

// Build sensor objects
VL53L4CD sensor1(&DEV_I2C, xshut_pin_1);
VL53L4CD sensor2(&DEV_I2C, xshut_pin_2);

//this holds the measurement
VL53L4CD_Result_t results1;
VL53L4CD_Result_t results2;

void initSensor(VL53L4CD sensorX, uint8_t sensoradd)
{
 // Init sensor1
 //Set sensor address.
 sensorX.VL53L4CD_SetI2CAddress(sensoradd);
 // Configure VL53L4CD satellite component.
 sensorX.begin();
 // Switch off VL53L4CD satellite component.
 sensorX.VL53L4CD_Off();
 //Initialize VL53L4CD satellite component.
 sensorX.InitSensor();
 // Program the highest possible TimingBudget, without enabling the
 // low power mode. This should give the best accuracy
 sensorX.VL53L4CD_SetRangeTiming(200, 0);
 sensorX.VL53L4CD_SetOffset(-10);
 // Start Measurements
 sensorX.VL53L4CD_StartRanging();
}

//getSensor1Reading
void getSensor1Reading(uint8_t status, uint8_t NewDataReady)
{
 sensor1.VL53L4CD_On();
 Serial.println("Sensor 1 is on");
 if ((!status) && (NewDataReady != 0)) {
 // (Mandatory) Clear HW interrupt to restart measurements
 sensor1.VL53L4CD_ClearInterrupt();
 // Read measured distance. RangeStatus = 0 means valid data
 sensor1.VL53L4CD_GetResult(&results1);
 snprintf(report, sizeof(report), "Sensor 2: Status = %3u, Distance = %5u mm",
 results1.range_status,
 results1.distance_mm);
 Serial.println(report);
 }
 sensor1.VL53L4CD_Off();
 Serial.println("sensor 1 is off");
}

//getSensor2Reading
void getSensor2Reading(uint8_t status, uint8_t NewDataReady)
{
 sensor2.VL53L4CD_On();
 Serial.println("Sensor 2 is on");
 if ((!status) && (NewDataReady != 0)) {
 // (Mandatory) Clear HW interrupt to restart measurements
 sensor2.VL53L4CD_ClearInterrupt();
 // Read measured distance. RangeStatus = 0 means valid data
 sensor2.VL53L4CD_GetResult(&results2);
 snprintf(report, sizeof(report), "Sensor 2: Status = %3u, Distance = %5u mm",
 results2.range_status,
 results2.distance_mm);
 Serial.println(report);
 }
 sensor2.VL53L4CD_Off();
 Serial.println("sensor 2 is off");
}

void setup() {
 uint8_t status;
 // Start the I2C Port and set its clock to 100kHz as the TOF sensors can't handle the faster clock speed of Arduino UNO R4
 Wire.begin();
 Wire.setClock(100000); 

 // Initialize the pinMode for the pins
 pinMode(ledPin, OUTPUT);
 pinMode(gpio_pin_1, INPUT_PULLUP);
 pinMode(gpio_pin_2, INPUT_PULLUP);
 attachInterrupt(gpio_pin_1, measure, FALLING);
 attachInterrupt(gpio_pin_2, measure, FALLING);

 // Initialize Serial Bus to write to console.
 SerialPort.begin(115200);
 // Wait until serial is booted up to continue.
 while (!Serial) {delay(20);}

 // Start the I2C bus
 SerialPort.println("Starting Serial I2C Bus");
 DEV_I2C.begin();
 delay(100);

 SerialPort.println("Initializating Sensors");
 initSensor(sensor1, sensor_1_address);
 initSensor(sensor2, sensor_2_address);
 

 SerialPort.println("Completed initialization of sensors");
}

void loop() {
 Serial.println("top of loop");
 // put your main code here, to run repeatedly:
 digitalWrite(ledPin, HIGH);
 uint8_t NewDataReady1 = 0;
 uint8_t NewDataReady2 = 0;
 uint8_t status1;
 uint8_t status2;
 do {
 Serial.println("check whether ready");
 status1 = sensor1.VL53L4CD_CheckForDataReady(&NewDataReady1);
 status2 = sensor2.VL53L4CD_CheckForDataReady(&NewDataReady2);
 } while (!NewDataReady1 || !NewDataReady2);
 getSensor1Reading(status1, NewDataReady1);
 getSensor2Reading(status2, NewDataReady2);

 digitalWrite(ledPin, LOW);
 delay(100);
 Serial.println("bottom of loop");
}



I did some more snooping around and found that the units simply aren't having their I2C addresses changed, so I tried to manually change just a single unit (and leave the second off for the time being):

 DEV_I2C.begin();

 digitalWrite(xshut_pin_1, LOW);
 digitalWrite(xshut_pin_2, LOW);
 digitalWrite(xshut_pin_1, HIGH);
 sensor1.VL53L4CD_SetI2CAddress(sensor_1_address);
 sensor1.begin();
 sensor1.VL53L4CD_Off();
 sensor1.InitSensor();
 sensor1.VL53L4CD_SetRangeTiming(200, 0);
 sensor1.VL53L4CD_StartRanging();

And the sensor is just returning the default I2C address that the unit comes with (0x29).

What gives here? Am I doing something wrong? I tested this with an R3 Uno, and got the same results.

Wire diagram for reference:

Untitled-drawing

This topic has been closed for replies.

4 replies

Graduate
Aug 25, 2025 3:54 PM UTC

Once you've changed the address of the sensor, don't turn it off. It will revert to the default address. 

To accomplish what you want ...

Put both sensors in reset by dropping the Xshut line - or the power I suppose. 

Then bring the first one out of reset. 

Change the address - and perhaps do the init.

Then bring the second one out of reset. 

And change its address and do the init.  

If this second sensor is the last one, you could just run without the address change, but I generally change the address of all the devices.

If either of the devices reboot - due to a power glitch or something - they will revert to the default address.

But the import bit is that if you drop the XShut or power them down, they will revert to the 0x29 default address. 

- john

"If this or any post solves your issue, please mark them as ""Accept as Solution"". It really helps the next guy.And if you notice anything wrong do not hesitate to ""Report Inappropriate Content"".I am a recently retired ST Employee. My former username was John E KVAM."
eclemmonAuthor
Associate II
Aug 25, 2025 4:14 PM UTC
 // Start the I2C bus
 SerialPort.println("Starting Serial I2C Bus");
 DEV_I2C.begin();

 // Put both sensors in reset by dropping the xshut lines
 digitalWrite(xshut_pin_1, LOW);
 digitalWrite(xshut_pin_2, LOW);
 // Bring the first one out of reset
 digitalWrite(xshut_pin_1, HIGH);
 // Change the address
 sensor1.VL53L4CD_SetI2CAddress(0x54);
 // If I don't init the software hangs, if I do, the first device is still at 0x29
 sensor1.begin();
 sensor1.InitSensor();
 sensor1.VL53L4CD_SetRangeTiming(200, 0);
 sensor1.VL53L4CD_StartRanging();

Hi John, thanks for the response. I'm still getting the same result even when I hard code the I2CAddress here—my I2C monitor is returning 0x29 as the address.

eclemmonAuthor
Associate II
Aug 25, 2025 4:58 PM UTC

I dramatically simplified my code and wiring and am still getting no change to the I2C address.

#include <Arduino.h>
#include <Wire.h>
#include <vl53l4cd_class.h>
#include <string.h>
#include <stdlib.h>
#include <stdio.h>
#include <stdint.h>
#include <assert.h>
#include <stdlib.h>

// Define I2C bus
#define DEV_I2C Wire
// Define Serial Port
#define SerialPort Serial
// Define xshut pin
#define xshut_pin 7

// New Address for sensor
uint8_t sensor_1_address = 0x54;

VL53L4CD sensor1(&DEV_I2C, xshut_pin);


void setup() {
 // put your setup code here, to run once:
 Wire.begin();
 Wire.setClock(100000);
 // Initialize Serial Bus to write to console.
 SerialPort.begin(115200);
 while (!Serial) { delay(20); }

 SerialPort.println("Starting Serial I2C Bus");
 DEV_I2C.begin();

 pinMode(xshut_pin, OUTPUT);

 digitalWrite(xshut_pin, LOW);
 delay(20);
 // Bring the first one out of reset
 digitalWrite(xshut_pin, HIGH);
 // Change the address
 delay(20);
 sensor1.VL53L4CD_SetI2CAddress(sensor_1_address);

 sensor1.begin();
 sensor1.InitSensor();
 sensor1.VL53L4CD_SetRangeTiming(200, 0);
 sensor1.VL53L4CD_StartRanging();

}

void loop() {
 byte error, address;
 int nDevices;

 Serial.println("Scanning...");

 nDevices = 0;
 for (address = 1; address < 127; address++) {
 // The i2c_scanner uses the return value of
 // the Write.endTransmisstion to see if
 // a device did acknowledge to the address.
 Wire.beginTransmission(address);
 error = Wire.endTransmission();

 if (error == 0) {
 Serial.print("I2C device found at address 0x");
 if (address < 16)
 Serial.print("0");
 Serial.print(address, HEX);
 Serial.println(" !");

 nDevices++;
 } else if (error == 4) {
 Serial.print("Unknown error at address 0x");
 if (address < 16)
 Serial.print("0");
 Serial.println(address, HEX);
 }
 }
 if (nDevices == 0)
 Serial.println("No I2C devices found\n");
 else
 Serial.println("done\n");

 delay(5000); // wait 5 seconds for next scan
}

 

Graduate
Aug 25, 2025 6:43 PM UTC

Do your functions check for a return? There is a possibility that the I2C function failed to set the address. 

If the device is booted and the I2C works, it really must work. It's only setting a register. So the 0x52 hits the bus, the 2-byte register address and then the one-byte new address. 

So first thing is to verify the I2C is working. Read the deviceID. And example of how to do this is in VL53L4CD API you can download from ST.com. 

But until you get this worked out, please check the completion status of the I2C read and write functions.

That has got to be the failure area.

- John 

"If this or any post solves your issue, please mark them as ""Accept as Solution"". It really helps the next guy.And if you notice anything wrong do not hesitate to ""Report Inappropriate Content"".I am a recently retired ST Employee. My former username was John E KVAM."