The easy thing to do here is to just buy the L1. It has the ULD you want. It is, however, more expensive.
But I can tell you a secret. The L3 is an L1 with the lens removed. So you can use the L1 ULD on the L3 - if you modify the function that checks the chipID.
(Note that without the lens, the ROI functions really have no meaning so don't use those.)
If you do this, you will not get the range that the data sheet promises. Probably only get a couple of meters.
(This is not encouraged, and you are kind of on your own if you try this.)
But if that is enough, then go for it.
The VL53L4CD is our least expensive ToF sensor, uses a very small driver and has a range of 1.3 meters. It has a narrower Field of View (18 degrees vs 27 degrees) that some people like. You might consider that one.
- john
If this or any post solves your issue, please mark them as 'Accept as Solution' It really helps. And if you notice anything wrong do not hesitate to 'Report Inappropriate Content'. Someone will review it.