Skip to main content
UDi T.1
Visitor II
December 9, 2021
Question

Reading distances with VL6180X on the workflow of one shot measurement "Wait for range measurement to complete" SYSTEM__INTERRUPT_CONFIG_GPIO it don't comes set never. what can be the reason?

  • December 9, 2021
  • 1 reply
  • 652 views

..

This topic has been closed for replies.

1 reply

John E KVAM
ST Employee
December 15, 2021

The 6180X is kind of robust but the most common issues are:

  • Poor power.
  • noise on the GPIO0 (Shutdown line) - this puts the sensor into reset and makes mess - a good sized pull-up is recommended.
  • -miss-configured I2C. This is easy to do. Always check the status on all your calls. An i2C failure will show up as a timeout.

But do look at the chip, if it's running you will see the laser - unless you are a bit old. Then use a laptop camera to view the laser.

Good luck,

  • john

If this or any post solves your issue, please mark them as 'Accept as Solution' It really helps. And if you notice anything wrong do not hesitate to 'Report Inappropriate Content'. Someone will review it.