Skip to main content
Visitor II
December 16, 2024
Solved

Questions about IOVDD and AVDD circuits in VL53L7CH sensors

  • December 16, 2024
  • 1 reply
  • 715 views

Hello.

I am designing a product using the VL53L7CH model.

I am using a 3.3V MCU.
So I'm trying to use 3.3V for both IOVDD and AVDD's voltage level.
Is there no problem if I use the same line without distinguishing IOVDD and AVDD?

 

Regards,

KORM

This topic has been closed for replies.
Best answer by John E KVAM

That is absolutely fine. A bit of care not to exceed the max voltage would be recommended. But it will be very happy running at 3v3 for both the AVDD and the IOVDD. 

- john

1 reply

John E KVAM
John E KVAMBest answer
ST Employee
December 16, 2024

That is absolutely fine. A bit of care not to exceed the max voltage would be recommended. But it will be very happy running at 3v3 for both the AVDD and the IOVDD. 

- john

If this or any post solves your issue, please mark them as 'Accept as Solution' It really helps. And if you notice anything wrong do not hesitate to 'Report Inappropriate Content'. Someone will review it.