Skip to main content
mf101
Associate III
March 1, 2021
Question

Question regarding VL53L1X_StopRanging()

According to the VL53L1X ULD API description when Vl53L1X_StopRanging() is called, an active ranging operation will be completed.

In a practical evaluation we tried to investigate whether an interrupt could still occur after calling this function or not:

-         we set a long timing budget

-         and called VL53L1X_StopRanging() + VL53L1X_ClearInterrupt() during ranging

An interrupt was never observed in this evaulation, which leads me to the question:

Is the API completing the ranging operation but not indicating the interrupt when the stop function is called during ranging ?

Unfortunately, the API description does not provide any information about this use case.

This topic has been closed for replies.

4 replies

John E KVAM
ST Employee
March 1, 2021

I don't know the answer to that. It never occurred to me to check.

There is bunch of logic controlling the ranging. It's way too fast to be able to control it with an MCU. That's why the stop command does not interrupt the ranging operation.

But the interrupt is under MCU control, and the MCU has already gotten the STOP command.

So when the range completes, it could well be that the MCU decides the interrupt is not required and simply waits for the next command.

I'll have to find the chip designer and see if I can get more information.

If this or any post solves your issue, please mark them as 'Accept as Solution' It really helps. And if you notice anything wrong do not hesitate to 'Report Inappropriate Content'. Someone will review it.
mf101
mf101Author
Associate III
March 2, 2021

Thanks for your response, it would be nice if you can get more information from the chip designer.

John E KVAM
ST Employee
March 9, 2021

I had my test team look at the lack of an interrupt after a stop.

And yes, after the stop, and the range ends, there is indeed no interrupt issued.

I sure hope this isn't a really big issue, as it cannot be changed.

One wonders however if after a stop one can poll the chip and get the last answer that way.

  • john

If this or any post solves your issue, please mark them as 'Accept as Solution' It really helps. And if you notice anything wrong do not hesitate to 'Report Inappropriate Content'. Someone will review it.
mf101
mf101Author
Associate III
March 10, 2021

Thanks for the clarification and your effort.