programming FOV
- 9 replies
- 4174 views
we are using the early version 1x in a vertical detection mode. it has a 23 degree fov.
in some of our testing we determined we need more.. FOV
currently we tilt the board holding the TOF sensor to eliminate wasted FOV where the sensor would be projecting on a wall. tof mounted 8ft high on the wall, projecting down, so we have tilted the FOV out, so that the back edge of the FOV is parallel to the wall its mounted on.
the newer 5x/8x have bigger FOV.. 63 and 90 degrees..
we don't need that much, BUT I would like to detect on the outer edge, vs a smaller square
4x4 with edge against the exclusion zone. or 6x4 with the 4 edge against the exclusion zone.
pic attached, box mounted on wal, tof pointing down, zoom in on box,
pad layout and detection zone
is this possible?
we need 6-10ft of detection in a narrow band. maybe 20-24 inches wide.