John E KVAMBest answer
ST Employee
October 30, 2023
For some reason I could not see the screen shot, but I think I know the issue.
The GUI package downloads a binary that powers up the sensor, initializes it and makes it ready. There are then a few commands that come from the PC which are translated and sent to the sensor. One of them is the 'start' command. Data is then taken from the sensor, and sent back to the PC.
This binary is complied for the Nucleo-F401RE. And while it might run on other boards, the PIOs are going to be different.
The solution is to just buy the F401RE. it's 10 dollars. And use that to prove the sensor does what you need. After that, download the API and use the STM32CubeIDE including the XCUBE_TOF to build the code for your WB55RG.
- john
If this or any post solves your issue, please mark them as 'Accept as Solution' It really helps. And if you notice anything wrong do not hesitate to 'Report Inappropriate Content'. Someone will review it.