Skip to main content
LWill.3
Associate
April 28, 2021
Solved

Mounting VL6180-SATEL

Given that the VL6180-SATEL breakout board has no mounting holes, is there a preferred method to accurately and rigidly mount it in the desired position and parallel to the mounting surface?

I would prefer to have it removable, so a permanent adhesive does not appear to be the best solution.

Thanks

This topic has been closed for replies.
John E KVAM
John E KVAMBest answer
ST Employee
May 28, 2021

there are lots of companies that will sell you almost the same board. SparkFun and Pololu are but two. AdaFruit is another

You can get that sensor in dozens of different layouts.

One of them will work for you.

I googled "vl6180 board" and got lots of references.

  • john
If this or any post solves your issue, please mark them as 'Accept as Solution' It really helps. And if you notice anything wrong do not hesitate to 'Report Inappropriate Content'. Someone will review it.

2 replies

John E KVAM
John E KVAMBest answer
ST Employee
May 28, 2021

there are lots of companies that will sell you almost the same board. SparkFun and Pololu are but two. AdaFruit is another

You can get that sensor in dozens of different layouts.

One of them will work for you.

I googled "vl6180 board" and got lots of references.

  • john
If this or any post solves your issue, please mark them as 'Accept as Solution' It really helps. And if you notice anything wrong do not hesitate to 'Report Inappropriate Content'. Someone will review it.
LWill.3
LWill.3Author
Associate
June 3, 2021

Thanks John. I used the ST Satel boards (they are quite cost effective as you get two in a pack).

To mount, I removed the connector, which I don't need, and glued on a 30 x 9mm piece of plain FR4 at right angles to the Satel board on the same side as the sensor. I drilled 2 x m2 clearance holes in the FR4 to enable mounting.

I do think ST should have made the board slightly larger to include two mounting holes.

Lance