Skip to main content
AElgh
Associate III
May 21, 2023
Question

LoRaWAN-End-Node + VL53L4CD, Sleep issue

Hello, I'm using the LoRaWAN-End-Node example on an STM32WL55JC MCU to drive the VL53L4CD sensor.  

I would like to use the interrupt pin to get the data from the sensor.

what is happening is that once __WFI() in the getting data subroutine is executed (code below), the LoRaWAN cycle seems to be broken.

How can i embed the "Sleep until an interrupt" in the LoRaWAN cycle?

Thank you...

void VL53_data_interrupt(cData_t *sensordata)
{
	// static uint8_t i = 0;
 
	 while (meas_count < NUM_MEASUREMENTS)
	 {
	 __WFI(); // Wait for interrupt
 
	 if (IntCount != 0)
	 {
	 IntCount = 0;
 
	 /* (Mandatory) Clear HW interrupt to restart measurements */
	 VL53L4CD_ClearInterrupt(sensordata->Vl53_Dev);
 
	 /* Read measured distance. RangeStatus = 0 means valid data */
	 VL53L4CD_GetResult(sensordata->Vl53_Dev, &(sensordata->VL53_Res));
 
	 if (sensordata->VL53_Res.range_status == 0)
	 {
	 Arr_dist_mm[meas_count] = sensordata->VL53_Res.distance_mm;
 
	// printf("Distance = %3u mm\n", results.distance_mm);
 
	 Acc_Dist += sensordata->VL53_Res.distance_mm;
 
	 meas_count++;
	 }
	 }
	 }
 
	 uint32_t Av_Distance = Acc_Dist / NUM_MEASUREMENTS;
 
	 printf("Average distance = %5lu mm\n", Av_Distance);
 
	 meas_count = 0;
 
	 Acc_Dist = 0;
}

This topic has been closed for replies.

2 replies

Tesla DeLorean
Guru
May 21, 2023

You're trying to do this in an INTERRUPT ??

Need to come up with a method that does this statefully

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
AElgh
AElghAuthor
Associate III
May 25, 2023

The Interrupt is working fine until the Stop-Mode is enabled then a strange behavior starts to happen:

  • sensor data is captured only once :

As the XShut(Interrupt-Pin) gets triggered when the MCU 1st stars.

  • the data is wrong.

I can go with the busy-wait solution but I'm trying to optimize the power as much as possible.