Skip to main content
JGarrettW
Associate II
May 16, 2024
Solved

Light Characterization for VL53L8CH VCSEL

Hello,

I am trying to do some ray tracing simulation for your VL53L8CH in a specific environment. I was wondering if you have any data beyond the "Field of Illumination" diagram for your VCSEL emitter (I assume you make your own emitters in-house). An "IESNA TM25" or "SPEOS" ray file would be amazing, but even just a maximum output power in lumens, watts, candelas, etc. would be helpful. That way I can at least know what the percentages in the "Field of Illumination" diagram mean. Also, if you have any detailed CAD on your chip that would allow me to place the emitter in the correct location on the sensor, that would be helpful as well. I have recreated it from your datasheet, but that doesn't have details on how deep the VCSEL is or what shape it is.

Thanks,

Garrett

This topic has been closed for replies.
John E KVAM
John E KVAMBest answer
ST Employee
May 22, 2024

I don't have any open data on that. What concerns us is the amount of energy that can pass through a 7mm aperture at a distance of 10cm. The 7mm is about the opening in your eye, and the 10cm is about the closest point you can focus. 

(We did not pick these numbers; the FDA and European heath organizations did.)

The trick was to not exceed the danger point, assuming the energy coming through that aperture was focused by your eye into one spot on the retina. 

It is this power that defines Class 1, and we are about, "20 times below the AEL of Class 1".

The output power of the VCSEL hardware itself, is kind of a closely guarded bit of competitive information. 

It's not something we can post on a forum. 

Sorry about that.

- john

If this or any post solves your issue, please mark them as 'Accept as Solution' It really helps. And if you notice anything wrong do not hesitate to 'Report Inappropriate Content'. Someone will review it.

6 replies

Anne BIGOT
ST Technical Moderator
May 21, 2024

Hello Garrett

ST is providing Field of Illumination datas only.

Anyway, you can find CAD design on st.com with a 3D STEP file with cones. 
For the VL53L8CH, you can find it here. Choose SamacSys model and you will be able to download the 3Dfile.

Hope this help,

 

Our community relies on fruitful exchanges and good quality content. You can thank and reward helpful and positive contributions by marking them as 'Accept as Solution'. When marking a solution, make sure it answers your original question or issue that you raised. ST Employees that act as moderators have the right to accept the solution, judging by their expertise. This helps other community members identify useful discussions and refrain from raising the same question. If you notice any false behavior or abuse of the action, do not hesitate to 'Report Inappropriate Content'
JGarrettW
JGarrettWAuthor
Associate II
May 21, 2024

Do you at least have what maximum power the field of illumination is referring to? 70% doesn't give me enough information to know how much loss to expect in certain environments.

John E KVAM
ST Employee
May 21, 2024

Knowing what the sensor can do in the presence of sunlight is a really tricky question. 

If the sun is directly behind the target, yet somehow is not shaded by the target, the loss is pretty high depending on the angle of the sun. Worst case is having the sun behind the sensor and illuminating the target. 

So, it's not only the Lux level, but the angle of the sun. 

The reason is we have an array of Single Photon Avalanche Diodes. And every photon that hits them gets counted. 

the sensor works because everything except the 940nm light gets filtered out.

But there is a non-zero reset time. 

So, if the sun - which generates a huge amount of 940nm light - saturates the max value the SPADs can receive, there is no bandwidth for the real signal. 

Oddly, if the sun is 90 degrees to the sensor, the results are better. 

But all of this depends on the reflectivity of the target. One wants a reflective target to get a good signal, but that reflectivity also reflects the sunlight. So, the sweet-spot is kind of hard to find.

Best I can tell you is to experiment a lot and see if it works for you. 

- john

If this or any post solves your issue, please mark them as 'Accept as Solution' It really helps. And if you notice anything wrong do not hesitate to 'Report Inappropriate Content'. Someone will review it.
JGarrettW
JGarrettWAuthor
Associate II
May 22, 2024

This is a zero-sun environment. What I am simulating is loss in an optical system (fiber optic cables, mirrors, etc.). For that, I need to know the initial power sent out by the VCSEL, the wavelength (940 nm), and the characteristics of my equipment.

John E KVAM
John E KVAMBest answer
ST Employee
May 22, 2024

I don't have any open data on that. What concerns us is the amount of energy that can pass through a 7mm aperture at a distance of 10cm. The 7mm is about the opening in your eye, and the 10cm is about the closest point you can focus. 

(We did not pick these numbers; the FDA and European heath organizations did.)

The trick was to not exceed the danger point, assuming the energy coming through that aperture was focused by your eye into one spot on the retina. 

It is this power that defines Class 1, and we are about, "20 times below the AEL of Class 1".

The output power of the VCSEL hardware itself, is kind of a closely guarded bit of competitive information. 

It's not something we can post on a forum. 

Sorry about that.

- john

If this or any post solves your issue, please mark them as 'Accept as Solution' It really helps. And if you notice anything wrong do not hesitate to 'Report Inappropriate Content'. Someone will review it.
JGarrettW
JGarrettWAuthor
Associate II
May 23, 2024

Ah, I understand the need to keep it guarded. Thanks for explaining it to me. That at least gives me a rough ballpark for simulation.