Skip to main content
VAkul.1
Associate II
August 30, 2021
Question

Laser TOF Sensor (VL53L1CXVOFY/1) power supply?

Hi, We are using Laser TOF Sensor (VL53L1CXVOFY/1) in one of our products.

Can we use AVDD=1.8V power supply? Even though AVDD = 2.8V, it looks like IOs will work on 1.8V.

This topic has been closed for replies.

3 replies

Mike_ST
ST Technical Moderator
August 30, 2021

Hi,

>> Can we use AVDD=1.8V power supply?

Please follow the datasheet if you want the device to operate normally:

Table 14. Recommended operating conditions

2.6V < AVDD < 3.5V

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. 
VAkul.1
VAkul.1Author
Associate II
September 15, 2021

Hi Mike,

Laser TOF Sensor (VL53L1CXVOFY/1) power supply?

If we connect AVDD (Pin 11) and AVDDVCSEL (Pin 1) to 2.8V, Are the IOs still operate on 1.8V mode as given in Datasheet page number 23, Table 14.

>The default driver mode is 1V8.

>2V8 mode is programmable using device settings loaded by the driver. For more details please refer to the

>VL53L1X API user manual (UM2356).

Regards,

Veera

Mike_ST
ST Technical Moderator
September 15, 2021

Please check the datasheet, there are 2 modes, "standard mode" which is (1.8V) and 2V8 mode :

https://www.st.com/resource/en/datasheet/vl53l1x.pdf

Section 5.2:

The default driver mode is 1V8. 

2V8 mode is programmable using device settings loaded by the driver. For more details please refer to the

VL53L1X API user manual (UM2356).

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.