Skip to main content
PThom.3
Associate
October 11, 2021
Question

Interrupt reset on e.g VL6180X

I want to use the TOF unit to detect when a physical object is passing. The Threshold detection shall rise an interrupt signal which I use to initiate a function. As I understand the mentioned VL6180X, the interrupt must be cleared each time via an I2C command. In my application I want the interrupt to reset itself when the object has passed and the value is within the threshold limit. As an object is passing each second, I do not have time to reset the interrupt by the I2C bus. Is there another TOF where this can be done, or does anybody have a solution for this? Thanks in advance /Poul

This topic has been closed for replies.

2 replies

John E KVAM
ST Employee
October 11, 2021

1) unless you use the Ambient Light Sensor of the VL6180X, consider the VL6180V1 - it's cheaper, and is the exact same silicon.

2) When you use an interrupt every time the sensor triggers you will need to clear the interrupt and start again. If you didn't you would not get the next interrupt.

Don't worry about the time it takes to clear an interrupt. It's only 1 payload character. With overhead - only 3 bytes. Even the slowest I2C bus can handle that.

  • john
If this or any post solves your issue, please mark them as 'Accept as Solution' It really helps. And if you notice anything wrong do not hesitate to 'Report Inappropriate Content'. Someone will review it.
PThom.3
PThom.3Author
Associate
October 12, 2021

Hi John.

Thanks for your info. I will give it a try, but probaply I need to have a separate cpu to do this one task, as the 'maiin application cpu' also is handling Modbus and analog conversions. I did hope for a less expensive and simpler solution though.

regards

Poul