Skip to main content
ABran.4
Associate II
April 18, 2023
Question

in DS of VL53L5CX->description: "Multizone distance measurements are possible up to 8x8 zones with a wide 65° diagonal FoV which can be reduced by software." i tried but did not find details how FoV can be reduced by software. please advice

  • April 18, 2023
  • 4 replies
  • 1686 views

..

This topic has been closed for replies.

4 replies

John E KVAM
ST Employee
April 18, 2023

That statement is a little misleading. You are going to get an 8x8 structure of data with information on each zone. And the FoV is 45x45, making each zone about 5 degrees x 5 degrees. If you don't want the data in a particular area, just don't bother to look at it.

In my water level software I only look at the dozen or so zones in the center, the others not having much value.

Sorry for the confusion.

  • john
If this or any post solves your issue, please mark them as 'Accept as Solution' It really helps. And if you notice anything wrong do not hesitate to 'Report Inappropriate Content'. Someone will review it.
ABran.4
ABran.4Author
Associate II
April 18, 2023

thank you for the answer.

>>You are going to get an 8x8 structure of data with information on each zone. And the FoV is 45x45, making each zone about 5 degrees x 5 degrees.

can i assume that 4x4 structure of data will give me about 11 degrees for each zone\?

John E KVAM
ST Employee
April 18, 2023

Exactly. And if you want the 4x4, you can run at 60Hz, which some applications want.

If this or any post solves your issue, please mark them as 'Accept as Solution' It really helps. And if you notice anything wrong do not hesitate to 'Report Inappropriate Content'. Someone will review it.
ABran.4
ABran.4Author
Associate II
April 18, 2023

thank you John