Skip to main content
CHand.2
Associate
October 12, 2021
Question

I wish to use the VL6180 within a pressurised chamber. What pressure can the package withstand? Max pressure would be ~15bar.

..

This topic has been closed for replies.

2 replies

John E KVAM
ST Employee
October 13, 2021

I wouldn't do it that way. The sensor is not a solid block of plastic and silicon. It's a bit of silicon with a cap over it and it contains air.

There is a small hole to keep it from exploding during the reflow process, but I would not count on that in your application.

Is there any way to create a window into your chamber and put the sensor on the outside?

The sensor really needs a coverglass to keep the elements from fowling the raw, exposed silicon.

By having the sensor look through a window of some sort, you protect the sensor and the same time as solving your pressure problem.

  • john
If this or any post solves your issue, please mark them as 'Accept as Solution' It really helps. And if you notice anything wrong do not hesitate to 'Report Inappropriate Content'. Someone will review it.
CHand.2
CHand.2Author
Associate
October 14, 2021

Thanks for the reply. I thought that might be the case. Having a window in the pressure vessel was plan B.

Cheers

Chris