Skip to main content
kdass.1
Visitor II
November 28, 2022
Question

I wanted to insert a ToF sensor (VL53L4CD) in an anesthetic container, I wanted to know which types of glass are suitable with the sensor.

I wanted to insert a ToF sensor (VL53L4CD) in an anesthetic container, because of the influence of the anesthetic on the sensor I need to protect my sensor with a protective glass, I wanted to know which types of glass are suitable with the sensor (can sensor laser pass through them).

This topic has been closed for replies.

2 replies

Anne BIGOT
ST Technical Moderator
December 7, 2022

Hello

Indeed there is a lack in our documentation and the Application Note about the cover glass guidelines for the VL53L4CD is not yet available. Anyway, you can have a look to this one : VL53L1CX cover glass guideline. The VL53L1X is near enough in term of features to the VL53L4CD so you can have a look to its AN.

Regards

Our community relies on fruitful exchanges and good quality content. You can thank and reward helpful and positive contributions by marking them as 'Accept as Solution'. When marking a solution, make sure it answers your original question or issue that you raised. ST Employees that act as moderators have the right to accept the solution, judging by their expertise. This helps other community members identify useful discussions and refrain from raising the same question. If you notice any false behavior or abuse of the action, do not hesitate to 'Report Inappropriate Content'
John E KVAM
ST Employee
December 7, 2022

And I might also add that ALL the information on coverglasses applies to the VL53L4 as well.

As the lasers have the same frequency (940nm) and the shapes of the VL53L0, L3 and L4 are idenical, whatever works for one will work for all.

(The L1 can also use the same glass, but it's 0.5mm taller and just a touch wider and longer. So one would have to accomidate the size difference.) But the app note applies to them all.

If this or any post solves your issue, please mark them as 'Accept as Solution' It really helps. And if you notice anything wrong do not hesitate to 'Report Inappropriate Content'. Someone will review it.