Skip to main content
GL.1
Associate
March 17, 2021
Question

I am using VL53L1X ToF sensor. I am able to use Short and Long Distance modes but How can I configure the sensor to medium mode ?

..

This topic has been closed for replies.

2 replies

Julien NGUYEN
ST Employee
March 17, 2021

Hi,

What is the driver are using ? Actually we do have two version of the driver for the VL53L1X, stsw-img007 and stsw-img009. The 009 has only 2 distance modes, We did not implement the medium mode in this driver because there is no any benefit. The short mode has better ambient immunity but the max distance measurable is shorter while the long distance mode has a longer max distance measurable but less performant in ambient light.

Thanks

Julien

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
GL.1
GL.1Author
Associate
March 18, 2021

Hi,

The driver I am using is STSW-IMG010.

As we are using VL53L1X, we want to test the sensor in medium mode. Can you suggest driver that contains all the features (3 Distance modes, Interrupt), so that it will be useful for our project

Thanks,

Gayathri