Skip to main content
CLE.11
Visitor II
August 2, 2021
Question

I am trying to wire the VL53L1X-SATEL breakout board to a microcontroller (ESP32) yet the pinout is not clearly defined (even in the datasheet). Is VDD supposed to be the voltage input (between 2.8V and 5V) ?

If the VDD pin on the left (breakable) part of the breakout board actually is the input voltage, then there is a problem, for the voltage drops and it even causes a brownout.

This topic has been closed for replies.

1 reply

John E KVAM
ST Employee
August 9, 2021

VDD is indeed the input to the sensor - and between 2.8 and 3.3 works. 5V is too high. But if the large chip on the back side of the satellite board is stuffed it's a level shifter and this the satellite board can handle a wide voltage swing.

Enclosed is the schematic for that satellite board.

If this or any post solves your issue, please mark them as 'Accept as Solution' It really helps. And if you notice anything wrong do not hesitate to 'Report Inappropriate Content'. Someone will review it.