Skip to main content
Lead
Jun 14, 2021 3:34 PM UTC
Solved

How have best accuracy at short distances: VL6180 or VL6180X?

Hi!

I notice that in the datasheet of both VL6180 and VL6180X, there is EXACTLY the same plot of distance measurement. So that's leaving me to the question: Who is best for short distances, VL6180 or VL6180X?

Have a look at page 12/87 here:

Proximity and ambient light sensing (ALS) module (st.com)

And have a look at page 32/73 here:

VL6180-Datasheet.book (st.com)

Both same plot. Why?

I assume that VL6180X is better for short distances, but I can be wrong too?

This topic has been closed for replies.
John E KVAM
John E KVAMBest answer
ST Employee
Jun 15, 2021 2:28 PM UTC

They have the same plot because THEY ARE THE SAME PART - at least inside.

Please let me explain...

The VL6180X was custom built for the cell-phone industry. And they wanted a combo chip that did Time of Flight ranging and an Ambient Light Sensor.

But when we released the part to the open market lots of our customers wanted ranging, but had no use for the ALS.

Turns our the ALS is kind of expensive to calibrate, and there is a rather hard-to-source optical filter.

To meet the requirements of our new customers, we

  1. Plugged the ALS hole - if you look carefully you can even see the part-line where the hole used to be.
  2. Removed the optical filter,
  3. Stopped calibrating the ALS.
  4. Changed the name to the VL6180V1
  5. Lowered the cost as the part is now easier to produce.

But we left the silicon exactly the same and changed absolutely nothing else.

In fact you are free to enable the ALS on the VL6180V1 as the silicon is still in there - but don't expect it to do much except use a little power.

So to answer your question - Same part, same plot.

And no, you are not wrong.

Nice job reading the datasheets in such detail. Not everyone does that.

  • john

If this or any post solves your issue, please mark them as 'Accept as Solution' It really helps. And if you notice anything wrong do not hesitate to 'Report Inappropriate Content'. Someone will review it.

2 replies

John E KVAM
John E KVAMBest answer
ST Employee
Jun 15, 2021 2:28 PM UTC

They have the same plot because THEY ARE THE SAME PART - at least inside.

Please let me explain...

The VL6180X was custom built for the cell-phone industry. And they wanted a combo chip that did Time of Flight ranging and an Ambient Light Sensor.

But when we released the part to the open market lots of our customers wanted ranging, but had no use for the ALS.

Turns our the ALS is kind of expensive to calibrate, and there is a rather hard-to-source optical filter.

To meet the requirements of our new customers, we

  1. Plugged the ALS hole - if you look carefully you can even see the part-line where the hole used to be.
  2. Removed the optical filter,
  3. Stopped calibrating the ALS.
  4. Changed the name to the VL6180V1
  5. Lowered the cost as the part is now easier to produce.

But we left the silicon exactly the same and changed absolutely nothing else.

In fact you are free to enable the ALS on the VL6180V1 as the silicon is still in there - but don't expect it to do much except use a little power.

So to answer your question - Same part, same plot.

And no, you are not wrong.

Nice job reading the datasheets in such detail. Not everyone does that.

  • john

If this or any post solves your issue, please mark them as 'Accept as Solution' It really helps. And if you notice anything wrong do not hesitate to 'Report Inappropriate Content'. Someone will review it.
DMårtAuthor
Lead
Jun 15, 2021 10:10 PM UTC

Thank you!

Then it does not matter if I select VL6180X or VL6180 if I'm doing ranging.

By the way! VL6180 should have better laser diode because I find it useful to have a smal angle of light instead of 15 degrees. Just like a normal laser pointer.

Then VL6180 will be very useful for the industri.

I'm going to use a VL6180X or VL6180 for measureing distances for production industri.

STM32MP151AAC3 custom board with STM32-OS as operating system: https://github.com/DanielMartensson/STM32-ComputerSTM32MP257FAK3 custom board with STM64-OS as operating system: https://github.com/DanielMartensson/STM64-Computer