Skip to main content
NAmam.2
Associate III
Nov 13, 2020 8:17 PM UTC
Solved

Hello, I am just wondering about VL53L1CB range sensing solution for Liquid level detection, do you think the photons from Transmitter would get reflected from the Liquids? Please let me know your thoughts about it. Thanks, Naga.

..

This topic has been closed for replies.
John E KVAM
John E KVAMBest answer
ST Employee
Nov 13, 2020 9:17 PM UTC

Of all the liquids water is the most interesting. Basically because it's largely transparent. I used to say it doesn't work. But then a customer proved me wrong.

The trick is to use the VL53L1X and use it's zone capability. If you can find a narrow field of view that is perpendicular to the water, use that zone. It will have a much larger signal return, and It will be the most accurate.

With ripples, trurbid, or foammy water, the answer will be just fine for all the zones. But for still, clean water the only accurate zone will be the one with the largest signal return.

But yes, it will work.

Oil - even really black fuel oil is not a problem.

And being in a dark tank really helps.

Good luck,

  • john
If this or any post solves your issue, please mark them as 'Accept as Solution' It really helps. And if you notice anything wrong do not hesitate to 'Report Inappropriate Content'. Someone will review it.

2 replies

John E KVAM
John E KVAMBest answer
ST Employee
Nov 13, 2020 9:17 PM UTC

Of all the liquids water is the most interesting. Basically because it's largely transparent. I used to say it doesn't work. But then a customer proved me wrong.

The trick is to use the VL53L1X and use it's zone capability. If you can find a narrow field of view that is perpendicular to the water, use that zone. It will have a much larger signal return, and It will be the most accurate.

With ripples, trurbid, or foammy water, the answer will be just fine for all the zones. But for still, clean water the only accurate zone will be the one with the largest signal return.

But yes, it will work.

Oil - even really black fuel oil is not a problem.

And being in a dark tank really helps.

Good luck,

  • john
If this or any post solves your issue, please mark them as 'Accept as Solution' It really helps. And if you notice anything wrong do not hesitate to 'Report Inappropriate Content'. Someone will review it.
NAmam.2
NAmam.2Author
Associate III
Nov 16, 2020 3:45 PM UTC

Thank you John for the information. Very helpful.

-Naga.