Skip to main content
Senior II
November 15, 2022
Question

HardFault_Handler when executing function GW_run from the guesture control static lib.

Hi,

I use the VL53L5CX in my own developped board .

Everything seems to work, but i can't get the guesture control code from static lib libGesturesMZ.a working (downloaded from STM website).

Initialisation goes fine , all statusses are OK , but the moment i run GW_run(....) the STM goes in HardFault_Handler().

All parameters i send with GW_run are valid and contain data .

Are there people that had the same problems?

Anything i can do to figure out why this is crashing?

these are the steps in software, all steps execute fine with STATUS_Ok but at GW_run() it crashes.

1) vl53l5cx_init

2) gesture_library_init_configure();

-> GW_init(&gest_predictor, &hand_tracker, &sensor_data);

-> HT_set_square_resolution(&hand_tracker, &sensor_data, Params.Resolution);

-> GW_set_frequency(&gest_predictor, &hand_tracker, &sensor_data, 1000.0/Params.RangingPeriod);

-> GW_set_params(&gest_predictor,....

-> GW_set_frequency(&gest_predictor, &hand_tracker, &sensor_data, 1000.0/Params.RangingPeriod);

-> SEN_set_orientation(&sensor_data, Params.SensorOrientation);

3) apps_layer_vl53l5cx_Configure(&L5Dev, &Params);

-> vl53l5cx_set_resolution(p_l5_dev, p_Params->Resolution==16 ? VL53L5CX_RESOLUTION_4X4 : VL53L5CX_RESOLUTION_8X8);

-> vl53l5cx_set_ranging_frequency_hz(p_l5_dev, (1000/p_Params->RangingPeriod));

-> vl53l5cx_set_integration_time_ms(p_l5_dev, p_Params->IntegrationTime);

-> vl53l5cx_set_xtalk_margin(p_l5_dev, 50);

-> vl53l5cx_set_target_order(p_l5_dev, VL53L5CX_TARGET_ORDER_CLOSEST);

-> 

4) vl53l5cx_start_ranging(&L5Dev);

5) loop

  {

vl53l5cx_check_data_ready(&dev,&IsReady);

if(IsReady == 1){

vl53l5cx_get_ranging_data(&L5Dev, &RangingData);

SEN_CopyRangingData(&sensor_data, &RangingData);

GW_run(&gest_predictor, &hand_tracker, &sensor_data); -> crash

}

  }

when looking at the hw registers after the crash bfsr_preciserr seems to be set and hfsr_forced is set also.

The last address of the PC was pointing to xTaskIncrementTick() .. this is from RTOS .

 0693W00000WIfBiQAL.png0693W00000WIfBOQA1.pngThank you 

This topic has been closed for replies.

2 replies

John E KVAM
ST Employee
November 22, 2022

There are muliple complied libraries for different processors.

The code is STSW-IMG035, but there is a qualifier on them for the cortex M0, M3, M33, M4 and M7

I'm guessing there is a mis-match between the ARM chip you are using and the version of the code you have. Carefully check the documentation on which chip you have and compare that to the software you've got.

Good luck,

  • john
If this or any post solves your issue, please mark them as 'Accept as Solution' It really helps. And if you notice anything wrong do not hesitate to 'Report Inappropriate Content'. Someone will review it.
Julien NGUYEN
ST Employee
November 24, 2022

Thanks John

I'm working with Steve directly.

The gesture lib supposes to support M4 core. The customer is using a G4 series STM32 microcontroller.

I will talk to Yann,

Bye

Julien

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.