Skip to main content
CRett.1
Visitor II
January 10, 2023
Question

Generate interrupt with VL6180 while MCU is sleeping

EDIT: Figured it out, I had to run the VL6180 in continuous mode.

I'm using a VL6180 for hand detection. I've successfully set up the interrupt at a certain range and it works nicely when the MCU is running. When the MCU is not running (aka not polling the sensor), the GPIO1 is low. I've probed it both connected and disconnected from the MCU to make sure it's not be influenced. Can the VL6180 generate the interrupt by itself?

This topic has been closed for replies.

1 reply

Anne BIGOT
ST Technical Moderator
January 10, 2023

Thank you for your interest for ST products.

Indeed running the VL6180 in continuous mode will fix the issue.

Our community relies on fruitful exchanges and good quality content. You can thank and reward helpful and positive contributions by marking them as 'Accept as Solution'. When marking a solution, make sure it answers your original question or issue that you raised. ST Employees that act as moderators have the right to accept the solution, judging by their expertise. This helps other community members identify useful discussions and refrain from raising the same question. If you notice any false behavior or abuse of the action, do not hesitate to 'Report Inappropriate Content'