Skip to main content
Visitor II
Jul 9, 2026 4:21 AM UTC
Solved

error code 7 when using VL53L1CB to measure the liquid water level

Hi, there,
we recently development a set up using vl53L1CB to measure water level.
During our test the sigal noise ratio is pretty good(1000/1), however, we got a very close distance (20-30mm) at real distance around 6-8m. Similar phenomenon did not occur at solid surface even at 8m.

And also, since we got a pretty good measurement at 8m with a solid surface, is there any possibility that we can break the firmware limit to reach a even longer distance?


Is there any possible suggestion?
thank you

BinBest answer
ST Technical Moderator
Jul 14, 2026 8:35 AM UTC

Hi:

can you upload the log data and basic setting of L1CB sensor when error code 7 occurs? Thanks.

if the final event print status=7, it means VL53L1_RANGESTATUS_WRAP_TARGET_FAIL (Wrapped target not matching phases).

 

In addition, according to the Ranging performances of the VL53L1 - Application note, the max ranging distance can reach up to 800cm, this is the maximum ranging capability while ensuring the safety of the laser.

Best regards,

Bin FAN

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.

1 reply

BinBest answer
ST Technical Moderator
Jul 14, 2026 8:35 AM UTC

Hi:

can you upload the log data and basic setting of L1CB sensor when error code 7 occurs? Thanks.

if the final event print status=7, it means VL53L1_RANGESTATUS_WRAP_TARGET_FAIL (Wrapped target not matching phases).

 

In addition, according to the Ranging performances of the VL53L1 - Application note, the max ranging distance can reach up to 800cm, this is the maximum ranging capability while ensuring the safety of the laser.

Best regards,

Bin FAN

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.