Skip to main content
MKlag.1
Associate
March 22, 2023
Question

Effect of "timing butget" using VL53L1CX

I use the "short mode" and set the timing butget to 100 ms. Every second I start a new measure with VL53L1X_StartRanging. With VL53L1X_GetRangeStatus() I poll for a new measure. But when I measure the time that is needed for a range it is only 20 ms. When I check this in ULD example I see the same, but the time is here 50 ms. Have I missunderstood something wrong?

This topic has been closed for replies.

2 replies

John E KVAM
ST Employee
March 22, 2023

20ms is kind of the default. So something went wrong with your setting.

Theory is that you do the 'init', you change the settings, and then issue the 'go' command.

Did you check the status return on all your calls? (not everyone does.)

but the TimingBudget does not really depend on the distance mode. So that's not it.

Compare your code to the example code and try to figure out what is different about yours.

But if you want to range once a second for 100ms, you set the Timing Budget to 100ms and the intermeasurement period to 1 second.

You only need to start it once, it will run until you send a stop command, days or weeks from later - or never.

If this or any post solves your issue, please mark them as 'Accept as Solution' It really helps. And if you notice anything wrong do not hesitate to 'Report Inappropriate Content'. Someone will review it.
MKlag.1
MKlag.1Author
Associate
March 23, 2023

Thanks, you for the fast respons. You are right, changing the intermeasurement period to 1 second makes sence. I changed the code so that I now poll on the gpoi interrupt pin whithout using VL53L1X_GetRangeStatus() and I see the right timing.