Skip to main content
BMcGe.1
Associate
May 17, 2023
Question

Does the cross-talk calibration on a VL6180X sensor always need to be performed?

The calibration procedure for a VL6180X sensor states that the offset calibration does not need to be done if the sensor is within +/- 3mm for a specified target. Is there every a situation in which the cross-talk calibration procedure doesn't need to be performed?

Can ambient light impact my offset and cross-talk calibration values?

This topic has been closed for replies.

2 replies

Zhiyuan.Han
ST Technical Moderator
May 18, 2023

Hi BMcGe

​

Cross-talk is the the TOF emitted light bounce back from glass to receiver, so cross-talk calibration is needed if you add a cover glass on top of VL6180CX. ​

Ambien light contain 850nm light will affect calibration result, if the light doesn't have 850nm energy, there will be no risk.

Br

Zhiyuan.Han

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
BMcGe.1
BMcGe.1Author
Associate
May 18, 2023

Would calibrating the cross-talk when there is no cover glass cause any issues with the sensor's readings?