Skip to main content
Visitor II
Jun 22, 2026 9:38 AM UTC
Question

Cover Glass Coating for the single-zone Time‑of‑Flight sensor

  1. We refer to the coating requirements in the newly updated AN5231 Cover Glass Guidelines for Single-Zone Time-of-Flight Sensor.Section 4.3 states “Additional coatings are not recommended.” Section 5.2 states “IR ink can be used over exclusion areas.” Table 3 under Section 7 states “Adding ARC can improve transmittance.”There appears to be an inconsistency. How should we interpret this? Are ARC coatings and IR ink permitted?
  2. Per AN5231, Section 3.1 and 7 recommend an IR transmittance target of 87%, and Section 4.2 defines the minimum requirement as ≥85%. Could you advise if 85% transmittance meets compliance? Polycarbonate typically achieves ~85% IR transmittance and is included in the guideline’s recommended material list.If we apply ARC coating to boost transmittance, this brings us back to the first question.

 

 

 

 

1 reply

Billy OWEN
ST Employee
Jun 23, 2026 7:24 PM UTC

Hi ​@Suzhen 

 

This post has been escalated to the ST Online Support Team for additional assistance.  We'll contact you directly.

 

Regards,

Billy