Skip to main content
qqzlqqzlqqzl
Associate III
April 8, 2025
Solved

Compatibility and Risks of Using VL53L3CX Library to Drive VL53L1 Sensor

Hello ST team,

I am using the full API for the VL53L1 TOF sensor, and I noticed that there are two versions of the full library available. One library (en.STSW-IMG015 VL53L3CX_BareDriver_1.2.10) is named vl53lx_api.c, and the other library (STSW-IMG019 VL53L1CB_BareDriver_6.6.18.2652) is named vl53l1_api.c. My understanding is that the library with "vl53lx" in the name should be a universal library that works with all TOF sensors, right? Both of these libraries seem to work with the VL53L1 TOF sensor. Our product aims to be compatible with both the VL53L3 and VL53L1 sensors while saving Flash space. Is there any risk in using the en.STSW-IMG015 VL53L3CX_BareDriver_1.2.10 library to drive the VL53L1 sensor?

Thank you in advance for your reply.

This topic has been closed for replies.
Anne BIGOT
Anne BIGOTBest answer
ST Technical Moderator
April 14, 2025

Hello

Using the SW packages of one device with another one may work.
Anyhow, tests are done using a combination of SW+HW and that's what ST is selling.

 

Our community relies on fruitful exchanges and good quality content. You can thank and reward helpful and positive contributions by marking them as 'Accept as Solution'. When marking a solution, make sure it answers your original question or issue that you raised. ST Employees that act as moderators have the right to accept the solution, judging by their expertise. This helps other community members identify useful discussions and refrain from raising the same question. If you notice any false behavior or abuse of the action, do not hesitate to 'Report Inappropriate Content'

1 reply

Anne BIGOT
Anne BIGOTBest answer
ST Technical Moderator
April 14, 2025

Hello

Using the SW packages of one device with another one may work.
Anyhow, tests are done using a combination of SW+HW and that's what ST is selling.

 

Our community relies on fruitful exchanges and good quality content. You can thank and reward helpful and positive contributions by marking them as 'Accept as Solution'. When marking a solution, make sure it answers your original question or issue that you raised. ST Employees that act as moderators have the right to accept the solution, judging by their expertise. This helps other community members identify useful discussions and refrain from raising the same question. If you notice any false behavior or abuse of the action, do not hesitate to 'Report Inappropriate Content'